How can we help you today?

Configuration Methods for PowerLogic A3 Arc Flash Protection Relay

Issue:
How can PowerLogic A3 Arc Flash protection be configured for different protection schemes and system requirements?

Product:
PowerLogic A3 Arc Flash Protection Relay

Environment:
Switchgear installations requiring flexible configuration options.

Cause:
Incorrect configuration can lead to nuisance tripping or failure to operate during an arc flash event.

Resolution:
PowerLogic A3 offers three configuration methods:

  1. Rotary Switch & Push Button
    • Quick setup for single devices or small systems.
    • Two rotary switches set Protection Scheme (positions 1–6) and Light Group (positions 1–9).
    • Push button used for Install/Reset and entering Test Mode.
    • Default: Scheme #1, Light Group 1, Current Group 16.
  2. eSetup Easergy Pro Software
    • Requires REL52960 configuration cable.
    • Allows full parameter customization: Protection Scheme, Light Group, Current Group, Output Latch.
    • Supports saving/loading configuration files and advanced diagnostics.
  3. ArcEM Configurator in V321
    • Used when A3 operates as I/O peripheral of V321.
    • Centralized configuration for large systems.
    • Enables mapping of Light Groups (1–12) and Current Groups (13–16) for selective tripping.

Best Practices:

  • Always verify scheme and group settings before commissioning.
  • Use Test Mode to validate sensor wiring and logic without tripping breakers.
  • Change default passwords for cybersecurity.

Schneider Electric Saudi Arabia