EcoSet Config System requirements
Here are the requirements for a PC to run EcoSet Config :
1. Windows operating system only (no touch-based OS or mobile devices)
2. Chromium-based browser (Chrome or Edge; no Firefox or Safari)
3. Dedicated GPU (graphics card)
4. Minimum of 16 GB RAM
5. Only one VEGA tab or window open at a time
6. Screen resolution of 1920 × 1080