Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why printing EcoStruxure Control Expert project documentation doesn't work ?

Issue:

Why printing EcoStruxure Control Expert project documentation doesn't work ?


Product Line:

Modicon PLCs

Environment:

EcoStruxure Control Expert V16.0/16.1, Windows 10/11

Resolution:

To enable EcoStruxure Control Expert to print project documentation, you must disable the “Let Windows manage my default printer” option in the “Printers & Scanners” settings.

Windows 10:

Screenshot 1

Windows 11:

Screenshot Windows 11