Why does slot 2 on the BMEXBP1200 and BMEXBP1002 backplanes NOT support Ethernet modules?
Why is slot 2 on the BMEXBP1200 backplane not a full-featured slot and unable to host Ethernet communication modules
Answer:
-
Issue
Customers report that when using the BMEXBP1200 12-slot backplane in Control Expert, slot 2 cannot accept Ethernet communication modules (e.g., NOR, NOC...). This often leads to confusion during rack configuration. - Resolution
This is not a defect but a design limitation of the BMEXBP1200 backplane.- Slot 2 is not Ethernet-capable; it only supports X Bus for certain module types.
- Ethernet communication modules must be installed in slots that support Ethernet and X Bus (slots other than slot 2).
Released for: Schneider Electric Saudi Arabia