How can we help you today?

What is the feature of "VLAN Qos Status "in NTSNEC1200 ?

Issue

What is the feature of "VLAN Qos Status "in NTSNEC1200 ?

Product Line

NTSNEC1200

Environment

Edge IO

Resolution

When this feature is activated ,the broadcast and TCP/UDP packets will be tagged with VLAN1 complying with M580 RIO network .

v1

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: