Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to print the logic of a project in Control Expert?

Article available in these languages: Spanish

Issue:

This FAQ explains the steps to print the project logic and provides tips for better organization.

Product:

EcoStruxure Control Expert (previously Unity Pro)

Environment:

PLC Configuration Software in Windows

Resolution:

To print the logic to a PDF, follow the steps shown in the image below:

1

Note: You can select which sections you want to print. In this example, all sections were selected.

2

Unfortunately, we are limited to a certain number of columns and rows (space) per page type. You can adjust the page setup and margins to fit as much of the logic as possible:

3

4

You can also enable Page Breaks to view how each page is divided. This feature helps you understand what content will appear on each page:

5

6

7

These are the available features you can use when working with the project printout.