Battery Compartment Screw Type for SEPAM 80 Protection Relay
Issue
Users need to identify the correct tool type and size required to open the battery compartment on the SEPAM 80 protection relay.
Product
SEPAM 80 Protection Relay
Environment
- SEPAM 80 relay front panel
- Battery compartment maintenance or battery replacement procedures
Cause
Misidentification of the screw head type on the SEPAM 80 battery compartment, leading to the incorrect assumptions.
Resolution
The battery compartment on the SEPAM 80 relay requires a TORX T08 driver to remove or fasten the screw properly. Using the correct TORX T08 tool ensures safe access to the battery compartment without damaging the screw head or the relay enclosure.