How can we help you today?

EcoStruxure IT Data Center Expert button to copy server ID is hidden.

Issue:
EcoStruxure IT Data Center Expert button to copy server ID is hidden

Product Line:
EcoStruxure IT Data Center Expert

Environment:
DCE 9.0

Cause:
The root cause of this is having high scaling settings in windows display options (175% scaling).

The server ID that IS visible in that window may also appear but may be missing a number of characters.

Resolution:
The user can override this by editing the DCE shortcut properties->compatibility mode->high dpi settings and selecting override scaling by system:

DPI_2

Schneider Electric Saudi Arabia