How can we help you today?

PowerChute Network Shutdown fails to power down ESXi host and records in the error log "cannot obtain HostSystem using findByIP or findByDnsName for critical host:"

Issue:

PowerChute error log reports "cannot obtain HostSystem using findByIP or findByDnsName for critical host:" for the configured ESXi host listed in the host protection page, and the host fails to power down.

Product:

PowerChute Network Shutdown

Environment:

PowerChute configured with VMware vCenter Server

Cause:

This concerns how the host's name appears in the vCenter inventory.

Example: The vCenter inventory lists the host as apc-esxi01.somedomain.com , while on the ESXi host, the hostname appears as APC-ESXI01. This mismatch causes the FindByDNSName API call to fail when issued against an ESXi host.

Solution:

Log in to each ESXi host via SSH and use esxcli to update the hostname to match what appears in vCenter:

esxcli system hostname set --fqdn apc-esxi01.somedomain.com

Schneider Electric Saudi Arabia