How can we help you today?

Smart UPS - 'Mains input bad' Event Messages after switching 3‑Phase input Source

Issue

The UPS logs the following events:

  • UPS: Main input bad. (0x01B0)
  • UPS: Main input bad cleared. (0x01B1)
  • UPS: Main input bad. (0x01B0)
  • UPS: Main input bad cleared. (0x01B1)
  • UPS: On battery power due to frequency and phase difference. (0x010)

These events typically occur when switching from a 3‑phase primary input source to a 3‑phase secondary source, such as a generator, or when switching back from the secondary source to the primary.

Both sources are accepted by the UPS when it is started on either one individually, and no issues occur when the input is changed to single‑phase.

Product Line

SRT8KRMXLI, SRT10KRMXLI

Environment

3 phase input with a secondary source

Resolution

This issue can arise when the phase order is different between the two input sources. At the start-up, the UPS will accept any phase sequence. But during the switchover, it's looking for the same sequence as previously receiving.

two sources showing incorrect and correct phase order

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: