Frequent Battery Transfers on Smart‑UPS Ultra 2.2 kVA & 3 kVA
Issue
Product Line
SRTL2K2RM1UIC
SRTL2K2RM1UINC
SRTL2K2RM1UC
SRTL2K2RM1UNC
SRTL3KRM1UIC
SRTL3KRM1UINC
SRTL3KRM1UC
SRTL3KRM1UNC
Environment
- Applies to UPS ID 1062 and UPS ID 1063
- Occurs when running UPS firmware earlier than version 05.1
Cause
Firmware versions prior to 05.1 include control changes introduced in firmware 04.9, which result in a higher sensitivity of the UPS to internal detection thresholds, causing more frequent transitions from on‑line to on‑battery.
Resolution
Firmware version 05.1 includes a revised algorithm that reduces the internal sensitivity threshold, significantly decreasing unnecessary transfers to battery. To ensure optimal behavior and overall system stability, upgrade the UPS firmware to the latest version available.
Released for: Schneider Electric Saudi Arabia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.