How can we help you today?

How to open the hardware configuration on a HMI programmed with EOTE?

Issue

It is not clear how to open the hardware configuration on a physical HMI programmed with EcoStruxture Operator Terminal Expert

Product Line

EcoStruxture Operator Terminal Expert

HMI running EOTE, EOTE Runtime

Resolution

There are 2 options to try and open the hardware configuration on an HMI running EOTE

[Option 1]

Display with Touch Gestures

Within 0.5 seconds, touch the top-right then bottom-left corners, or the top-left and bottom-right corners (within a 40 pixel area) of the screen

Open the hardware configuration with gestures

This option can be enabled / disabled from the settings as follows.

1/ In the Project Explorer window, from [System Architecture] click [Target01].

2/ In the Properties window, go to [Function] tab ➞ [Options] tab ➞ [Preference].

Display Hardware Configuration option in EOTE

[Option 2]

Display with Hardware Configuration object on a screen

Note: The size of the object is the size of the Hardware Configuration screen. It is not a button.

Hardware Configuration Tool Part

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia