How can we help you today?

BCIM Functionality Requirements with Micrologic Active

Make sure to use EPC 2.39 or above to upgrade Micrologic Active trip unit toFirmware version 004.004.003 or later

What happens if the Micrologic Active firmware is not updated?

You may experience issues such as:

  • BCIM not appearing in the EPC

  • Incorrect or missing measurement data

  • Communication errors on the trip unit

Note : Ensure 24V auxiliary supply provided to BCIM separately through the 6-Pin COM port.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation