How can we help you today?

Basic Documentation Resources for PowerLogic P5 Protection Relays

Issue

Users need to know which core documents are required to work with PowerLogic P5 relays.

Product

PowerLogic P5 Protection Relays

Environment

Medium‑voltage protection systems using P5 relays for feeder, transformer, motor, or line protection.

Cause

Users often lack clarity on the essential manuals needed for installation, configuration, and communication setup.

Resolution

The two essential documents for understanding, configuring, and integrating PowerLogic™ P5 relays are:

1. PowerLogic P5 User Manual
Covers the relay’s operation, protection functions, hardware, and configuration.
Link: https://www.se.com/us/en/download/document/P5_UserManual_EN_M/

2. PowerLogic P5 Communication Manual
Describes communication ports, protocol configuration (IEC 61850, Modbus, DNP3, etc.), and network architectures.
Link: https://www.se.com/us/en/download/document/P5_Communication_EN_M/

Schneider Electric Saudi Arabia