How can we help you today?

What information is available about the SRV36BP-9A, SRVS36BP‑9A, SRV36RLBP-9A and SRVS36RLBP-9A?

Issue:

What information is available about the SRV36BP-9A, SRVS36BP‑9A, SRV36RLBP-9A and SRVS36RLBP-9A?


Product Line:

SRV36BP-9A, SRVS36BP‑9A, SRV36RLBP-9A, SRVS36RLBP-9A?

Environment: All serial


Answer :

The SRV36BP-9A, SRVS36BP‑9A, SRV36RLBP-9A and SRVS36RLBP-9A battery pack is compatible with the Easy UPS 1 kVA range.
Please refer to the specific UPS model that the SRV36BP‑9A supports below.

battery info

See image below showing the actual measurement of the battery cable length (23.6 in).

battery cable

The SRV36BP-9A, SRVS36BP‑9A, SRV36RLBP-9A and SRVS36RLBP-9A has a battery breaker on the back with a maximum rating of 50 A. If you want to activate the voltage at the connectors, you need to switch it on.
see image below:
actual
battery breaker 1
Below is a diagram illustrating the internal battery connections of the SRV36BP-9A, SRVS36BP‑9A, SRV36RLBP-9A and SRVS36RLBP-9A . Consists of 6 individual batteries, each rated at 12 V DC.
battery string
For additional information, please refer to the link below:

SRV36BP-9A

https://www.se.com/id/en/product/SRV36BP-9A/apc-easy-ups-online-srv-battery-pack-1kva-for-extended-runtime-model-36v-648vah/

SRV36RLBP-9A

https://www.se.com/ph/en/product/SRV36RLBP-9A/apc-easy-ups-online-srv-36v-rm-battery-pack-for-1-kva-extended-runtime-model/

SRVS36RLBP-9A

https://www.se.com/eg/en/product/SRVS36RLBP-9A/easy-ups-online-srvs-rackmount-battery-pack-for-1kva-extended-runtime-model-36v/

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation