Troubleshooting SmartConnect-compatible UPS Connection to the Cloud
Issue 1: Troubleshooting the UPS Connection to the Cloud
- If you are having difficulty connecting your UPS to Schneider Electric cloud services, see Network Requirements.
- See Issue 2: APC Smart-UPS Device Types below to troubleshoot the connection of your APC Smart-UPS device.
Issue 2: APC Smart-UPS Device Types
There are three device types that can connect to Schneider Electric cloud services:
1. UPS with a Character Display
- Navigate to the Status menu.
- Navigate to SmartConnect:
Issue 3: UPS Connection Status Indicators
| UPS Character Display | UPS Icon Display | UPS Status Indicator | Description |
| No Ethernet | Sc.0 | Indicator not illuminated | The LED indicators above the Ethernet port are not illuminated. Action - Check that the Ethernet cable is firmly inserted into the Ethernet port by disconnecting it and reconnecting it. Once connected, the Ethernet port LED will illuminate. |
| Addressing | Sc.2 | N/A | The device is obtaining an IP address on the local network via DHCP. Action - If this is displayed for more than 2 minutes, check that the configuration of the DHCP server will allow the MAC address of the device. See Network Requirements. |
| Contacting | Sc.4 | N/A | The device is establishing a connection to Schneider Electric cloud services. Action - If this is displayed for more than 2 minutes:
|
| Securing | Sc.5 | N/A | The UPS is securing the TLS network connection. Action - If this is displayed for more than 2 minutes, ensure that the following cipher suites are not blocked in your firewall configuration: TLS_PSK_WITH_AES_128_CCM_8 TLS_PSK_WITH_AES_128_CBC_SHA256 TLS_PSK_WITH_AES_128_CBC_SHA If the above cipher suites are allowed and this status persists, contact APC Customer Support. |
| Connecting | Sc.6 | N/A | The UPS is establishing communication with Schneider Electric cloud services. Action - If this is displayed for more than 2 minutes, contact APC Customer Support. |
| Connected | Sc.1 | Green | The device has established a connection to Schneider Electric cloud services, and is operating normally. |
| Disabled | Sc.7 | Red | Action - Contact APC Customer Support. |
| Prohibited | Sc.8 | N/A | Ethernet connection is not allowed due to a hardware issue or configuration. Contact APC Customer Support. |
Issue 4: Restart the UPS Network Interface
| UPS models with the prefix SMT/SMX/SMTL To reset the network interface of an SMT/SMX/SMTL model UPS, on the display interface hold the UP and DOWN buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted. | |
| UPS models with the prefix SMC To reset the network interface of an SMC model UPS, on the display interface hold the MUTE and MENU buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted. | |
| UPS models with the prefix SCL To reset the network interface of an SCL model UPS, insert a paperclip into the Reset pinhole on the rear of the UPS. | |
| UPS models with the prefix SRTL To reset the network interface of an SRTL model UPS, on the touch screen interface navigate to Configuration > Communication > Smart Connect Restart > select Yes. |
Released for: Schneider Electric Saudi Arabia