Can't connect more than one OPC UA Clients to the BMENUA0100 module via Secure connection
Issue
The BMENUA0100 module can only connect to a single OPC UA Client via Secure Connection (certificate signed encryption). More than one connection cannot be established.
Product Line
BMENUA0100 / BMENUA0100H - OPC UA Embedded Module (Modicon X80 Platform)
Environment
OPC UA communication
Resolution
In Access Control -> User Management of the BMENUA0100 module, the 4 Authentication Roles are:
1) SECADM (admin)
2) OPERATOR
3) ENGINEER
4) INSTALLER (used for firmware updates from the EcoStruxure Automation Device Maintenance tool)
See the "Access Control" section of the "BMENUA0100 OPC UA Embedded Module, Installation and Configuration Guide"
https://www.se.com/us/en/download/document/PHA83350/
If there are MORE THAN ONE Users with the INSTALLER role configured, it causes the BMENUA0100 firmware to reject all but one OPC UA Client.
The firmware only allows one User to have the role of INSTALLER - but this limit is not reflected in the User Interface validation rules of the NUA Webpage.
So as long as you keep only a single user with the INSTALLER role, then you can have up to the maximum 15 simultaneous OPC UA Clients connected via Secure Mode.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for: Schneider Electric Saudi Arabia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.