How can we help you today?

PME - Management Console error "There was no endpoint listening"

Issue

Management Console doesn't open and shows "There was no endpoint listening at http://servername/23102/CoreServicesHost/InternationaIization/InternationaIizationService that could accept the message. This is often caused by an incorrect address or SOAP action. See InnerException, if present, for more details."

No endpoint listening error

Product Line

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Management Console

SQL Server

Cause

There is more than one server name listed in the ApplicationModules Inventory.ApplicationServer table.

Resolution

*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

1. Log into SQL Server Management Studio > Databases > ApplicationModules > Tables, then right-click on Inventory.ApplicationServer > Edit Top 200 Rows.

Multiple entries in Inventory.ApplicationServer

2. Copy the correct server name (in this example: SERVERNAME)

3. Edit the Name for ServerId 2 to a random name.

Edit ServerId name

4. Paste the correct server name into the Name column for ServerId 1.

Copy correct name to ServerId 1

5. Run the following script to delete the extra entry:

USE ApplicationModules

DELETE FROM Inventory.HostedService

WHERE HostID IN (SELECT HostID FROM Inventory.Host WHERE ServerID > 1)

DELETE FROM Inventory.Host WHERE ServerID > 1

DELETE FROM Inventory.ApplicationServer WHERE ServerID > 1

Schneider Electric Saudi Arabia

Attachment(s)
Remove extra Inventory.ApplicationServer entries.sql [238 Bytes]