How can we help you today?

Compact DAP212/252/253 to X80 DDM16025 quick wiring - 990XSM00205

Issue

Migrating an ASBDAP212/252/253 to a BMXDDM16025 and need to confirm the 990XSM00205 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation