How can we help you today?

Vijeo Designer: What is new regarding the HMI License Manager V2?

Vijeo Designer V6.3 SP3 comes with a new version of the HMI License Manager V2 including the way to activate a license by using the Offline Mode. The goal of this article is to inform about the expected behaviours after installing this version.

This article is applicable to the following products:

Vijeo Designer Build Time and Run Time

This topic is related to Vijeo Designer 6.3 SP3 or newer

Here is the Management of the Licensing with the new HMI License Manager V2

  • The HMI License Manager V1 was installed by the versions VJD V6.3 /SP1/SP2
  • VJD 6.3 SP3 installs the HMI License Manager V2 in parallel of the HMI License Manager V1 (there are 2 icons of the License Manager on the PC desktop after installation of VJD 6.3 SP3)
  • If a license of VJD V6.3 is already registered on the PC with the HMI License Manager V1, there is no update of the License registration after installation of VJD 6.3 SP3. It means that version V1 will continue to keep and manage the license.
  • At any time, it is possible to return the license from version V1 and then activate it into version V2.
  • If VJD V6.3 was already installed but no license was registered with the HMI License Manager V1, after installation of VJD 6.3 SP3 on the PC the License Manager V2 is available and the registration can be done, including the Offline Mode.
  • EcoStruxure Operator Terminal Expert V4.0/4.1/4.2 and Vijeo Designer 6.3 SP3 are now using the same HMI License Manager V2.

Below, please find some useful FAQs regarding the HMI License Manager V2:

    EcoStruxure Operator Terminal Expert: How to Activate/Deactivate a License for an Online Device with HMI License Manager?

    EcoStruxure Operator Terminal Expert: How to Activate a License for an Offline Device with HMI License Manager?

    EcoStruxure Operator Terminal Expert: How to Deactivate a License for an Offline Device with HMI License Manager?

    Schneider Electric Saudi Arabia