How can we help you today?

Is the ZBZ58 compatible with Harmony XALK control stations ?

The ZBZ58 bellows is not designed to be installed with a ZB4BZ1905 guard. Installing the bellows together with the guard may cause difficulties for the emergency stop head to automatically return to its initial position after reset. For this reason, such an installation is not recommended.

I have tested other guards as well, but unfortunately none of them is wide enough to allow proper operation of the emergency stop pushbutton when used with a bellows.