How can we help you today?

APC Surge Arrests and Back‑UPS: What’s Changed and Why

Question:
APC Surge Arrests and Back‑UPS: What’s Changed and Why

Product:
APC by Schneider Electric Surge Arrests


Environment:
All serial numbers

Answer:

What changed with APC surge protectors?

APC has not stopped protecting home electronics from power surges. Instead, surge protection is now included as part of more advanced products designed for today’s home power needs. Rather than offering surge protection as a separate device, APC focused on to further innovate Back‑UPS systems that will provide broader power protection.


Why did APC make this change?

Over time, how homes use electronics has changed. Many households now rely on computers, routers, smart TVs, streaming devices, and home networking equipment that are sensitive not only to surges, but also to power outages, low voltage, and unstable power. Back‑UPS products are designed to support these needs by providing protection and short‑term power backup when issues occur.


Does a Back‑UPS still protect against power surges?

Yes. Surge suppression and power filtering are built into Back‑UPS products. APC has incorporated its experience and design principles from earlier Surge Arrest and power‑filtering products into the Back‑UPS family.


What standards do Back‑UPS products follow?

Back‑UPS systems are designed and evaluated under recognized safety standards for uninterruptible power supplies, including UL 1778. Their surge protection functions are aligned with applicable requirements associated with UL 1449 (4th Edition). These standards help ensure products are designed for safety and tested appropriately for their intended use.


How is a Back‑UPS different from a basic surge protector?

A basic surge protector is designed to respond to certain electrical spikes. A Back‑UPS offers additional features, which may include:

  • Surge protection
  • Power filtering
  • Voltage regulation
  • Battery backup during brief outages

These added functions are intended to help keep connected devices running and to support proper shutdown during some power interruptions.


Is a Back‑UPS more expensive than a surge protector?

Back‑UPS products generally have a higher upfront cost because they include batteries and additional electronics. Many customers choose a Back‑UPS because it offers added peace of mind by protecting both equipment operation and, in some cases, unsaved work or data during power events.


Does APC still offer an Equipment Protection Policy?

Yes. Back‑UPS products continue to include an Equipment Protection Policy, subject to specific terms and conditions. This policy reflects APC’s commitment to supporting customers and protecting eligible equipment connected to APC UPS products. Details, limitations, and requirements are outlined in the official policy documentation.


Is a Back‑UPS necessary for every home?

Not every home needs the same level of protection. A Back‑UPS may be helpful for devices such as desktop computers, home offices, modems, routers, or entertainment systems where power interruptions could cause inconvenience or data loss. Customers are encouraged to review product specifications or consult APC resources to determine the most appropriate solution.


Where can I learn more or get help choosing a product?

Additional information is available on APC’s official website, including product guides, specifications, and support tools to help customers select a solution that fits their needs.

If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

End of Life Instructions for Surge Arrests can be found in this link or you can refer to the attached document.

Please also refer to the attached document that outlines the official letter of APC by Schneider Electric's decision to exit from the APC Surge Protection Market.

Schneider Electric Saudi Arabia

Attachment(s)
EoLI - Personal Surge Protectors.pdf [776.78 KB]
Schneider_Electric_Surge_Protection_Exit___External_Announcement_Final.pdf [845.76 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category:
  • Product Documentation