How can we help you today?

Video: How to upgrade the firmware for BMXNOM0200 module?

Use Unity Loader V2.2 and above to upgrade the NOM module. Make sure that Memory card in the CPU is in good condition else it will not allow to upgrade the firmware and will give Access Invalid error.

1

Select the Firmware Tab and Connect to PLC. Select the firmware file to be downloaded to the NOM. Select the proper location of the NOM module by selecting the rack and slot of NOM module.

2
The green color arrow shows the module firmware can be upgraded with the file selected in the PC. Press Transfer to transfer the selected file from PC to NOM. At last once upgraded it will show successful completion.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)