How can we help you today?

How to synchronize an M580 CPU in firmware 4.xx with a Windows machine NTP server

When a Windows PC is used to be the NTP server that will deliver time to an M580 CPU with firmware 4.xx it can happen that despite the NTP communication is established, the M580 doesn't update his clock. In that case a parameter inside the w32time register need to be modified and set to 0 as below :

BMENUA0100 vs Windows 10 NTP Server.PNG

Schneider Electric Saudi Arabia
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
  • Product Documentation