How can we help you today?

Can the customer use 1 AWG instead of 1/0 AWG for the ATV630D55N4, despite the installation manual specifying 1/0?

Issue:

Can the customer use 1 AWG conductors instead of 1/0 AWG for the ATV630D55N4, even though the installation manual specifies 1/0?

Product Line:

ATV630, ATV930

Environment:

Conductor size does not meet the required specification

Resolution:

We are not authorized to deviate from the requirements outlined in our installation manuals.

wire

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation