How can we help you today?

What level of ground fault protection does the ATV320 provide?

Issue:

What type and level of ground fault protection is implemented in the ATV320 drive?

Product Line:

ATV320

Environment:

Ground fault detection operating environment

Resolution:

There are two methods for ground fault detection according to drive size.

For small VSD size, the ground short circuit detection SCF3 is done by a current mirror on the DCBUS current.

The circuit detection compare the current on +DCBUS with the current on -DCBUS.

For bigger VSD size the ground short circuit detection SCF3 is done by homopolar current sensor.

The homopolar current sensor measures the unbalance between the three input phases.

For both methods, the threshold detection is 25% of the nominal inverter current.

This Threshold is fixed value for ATV320 and can't be adjusted.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: