How can we help you today?

What is the right method to handle the unused power cables on SNAP IN Busbar?

The power cables (flexible wires) on SNAP IN busbar are used to distribute the power from busbar to GV2(snap in version). They are fixed in the safety hole when delivery to customer.

- When select the SNAP IN busbar, please choose the proper busbar commercial reference whose number of tap-offs equals to number of GV2 which will be installed under the busbar, in this case, there won’t be unused power cable to be handled.

- In case number of GV2 is less than the number of tap-offs from busbar, please follow the Instruction sheet NAT1303101 to always keep all unused power cables inside the safety hole with the grey mark covered up, failure to follow these instructions can result in death, serious injury, or equipment damage.

One example:

There is one grey mark on the surface of the cable in image001 in red highlighted.

image001

image001

image002 is not OK because the grey marks on the surface of the wires are visible. Customer should push the cable more inside the holes.

image002

image002

image003 is OK because the grey marks on the surface of the wire are inside the holes.

image003

image003