How can we help you today?

How to Change Animation Display Colors in Control Expert

Overview
This article describes how to customize animation colors in EcoStruxure Control Expert when using Remote Connect. By modifying the Control Expert color configuration files, users can improve visibility and more easily differentiate between True and False logic states during online monitoring.
For example, users can configure:
•    False values to display in Black
•    True values to display in White
This customization helps improve readability of animated logic in Function Block Diagram (FBD) views.


  • The image below shows the default FBD animation appearance before any color modifications are applied.
    Before change
    Modify FBD Animation Colors
    To change the animation colors for Function Block Diagram (FBD):
    Locate and open the following configuration file, “FBDColors.ini”
    location
  • Open the file using a text editor.
    By default, the FBDColors.ini file contains the standard Control Expert color settings, as shown below.

before change

  • Modify the required color values for the desired animation states. An example configuration is shown below where:
    False state is configured as Black
    True state is configured as White
    updated file
    After updating the file:
    •    Save the changes
    •    Restart Control Expert for the new colors to take effect
    Once Control Expert restarts, the new animation colors will be displayed in the FBD view for the corresponding logic states.
    Update CE
    Example:
    •    False state → Black
    •    True state → White
    This allows the same inputs and animations to appear with customized color behavior.

    Additional Information
    This method can also be used to customize colors for other programming languages in Control Expert by modifying the corresponding .ini files:
    •    LDColors.ini → Ladder Diagram (LD) colors
    •    STColors.ini → Structured Text (ST) colors
    Users can edit the available fields defined in these .ini files to customize the display colors as needed.

Schneider Electric Saudi Arabia