How can we help you today?

How to retrieve project information/detail within the application in Control Expert

Issue :

How can I retrieve information like the major, minor and build version of a project within the application so that it can be read via Modbus

Product Line :

Control Expert (formerly Unity Pro)

Resolution :

The PRJ_VERS block from the System library would be the block to use for that.

function block

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: