How can we help you today?

Is my NMC 3 vulnerable to CVE-2000-0916 or CVE-2000-0328?

Issue:
A customer reports : "There is a Vulnerability on our NMC3's on CVE-2000-0916 or CVE-2000-0328"

Product Line:
AP9640 / AP9641

Resolution:

This is likely a false positive. The NMC is not vulnerable to CVE-2000-0916 or CVE-2000-0328 since it does not, and has never, used FreeBSD or NT 4.0.

If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Saudi Arabia