How can we help you today?

How do I setup Modbus serial communication between two Ecostruxure Machine Expert controllers using the Read_Var function block?

Issue:

How to setup Modbus serial communication between two Ecostruxure Machine Expert controllers using the Read_Var function block


Product Line:

Ecostruxure Machine Expert


Resolution:

In this example, the M251 is setup a Modbus Slave and the M262 as Master. Ensure that both devices serial line settings are identical

image1

Below is the logic where the blink function is used to execute the read every second.  The address table variable of the ADDM block must be used as the address(Addr pin) of the READ_VAR block. Attached is the sample project created in Ecostruxure Machine Expert V2.3

image2

Schneider Electric Saudi Arabia

Attachment(s)
M262_Master_M251_Slave_Read_Var_Modbus_Serial.project [740.38 KB]
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
Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Help Centre

Find support resources for all your needs, in one place.