How can we help you today?

PM5500, 5600 & 5700: How to access the Phasor Diagram feature

Issue

Customer would like to understand how to access the phasor diagram on the meter's physical display..

Product Line

PM5500, PM5600 & PM5700

Environment

Hardware

Cause

Finding the phasor diagram might not be intuitive to the user.

Resolution

To find the phasor diagram on the PM5500, PM5600 or PM5700, find the "Maintenance" button at the meter's home screen:

Home Screen

From the Maintenance screen, find the "Diag" button:

Maint Screen

From the Diag screen, navigate one section over using the arrow button:

Diag Screen

From the 2nd section in the Diag screen, find the "Phasor" button:

Diagnostics 2

This will take you to a phasor diagram of the application that your device is dedicated to monitoring.

Schneider Electric Saudi Arabia