How can we help you today?

Is an EMC filter included in the ATV320 M3C and S6C drive ranges?

Issue:

Could you please confirm whether the ATV320 M3C and S6C ranges are equipped with an EMC filter?

Product Line:

ATV320

Environment:

N/A

Resolution:

The information from installation manual is correct. There is no EMC filter on these range M3C and S6C.

The reason there is IT jumper in screw is because the external hardware is common with N4C range.

So keep IT jumper or removed has absolutely no difference for range M3C and S6C, as they are built without EMC filter.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: