How can we help you today?

Power Monitoring Expert (PME) System Health Tab in PME2024R3 Web Applications Shows Licensing Error

Issue:

After installing either the Cumulative Update from 2026-04 or 2026-06 for PME2024R3 there will be an additional tab added in the Web Applications called "System Health". This can be used to monitor additional things such as the RAM usage, disk space, Windows OS compatibility, database integrity and more.

However, when looking at the tab you may encounter a message "Unable to process the request. You are not Licensed to perform this action. Please see your system administrator. Try Again"

unable to process request


Product Line:
Power Monitoring Expert (PME) 2024 R3 Cumulative Update 2026-04

Power Monitoring Expert (PME) 2024 R3 Cumulative Update 2026-06

Environment:
Web Applications System Health Tab

Resolution:

First, to verify, open the License Configuration Tool on the server. Click on the License Information button within the tool as shown below. This will show the components of the licensing currently applied to the PME system.

license information in the license configuration tool

Within the License Information, look for the line "SystemHealthMonitor" within the components of the licensing. If present it will show as below:

systemhealthmonitor license addition to the licensing components

If this line within the Licensing Information is not present, please follow the process of returning and reactivating the license.

To return the license → How to return PME 2021 license online for license configuration tool | Schneider Electric USA

To activate the license → How to Activate Power Monitoring Expert License Offline Using MySchneider Portal | Schneider Electric USA

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: