How can we help you today?

PME 2024 R3 CM Tool - Backwards Compatibility

Issue

Customer would like to know the compatibility of the PME 2024 R3 CM Tool

Product Line

Power Monitoring Expert 2024 R3

Environment

Software / Upgrade / Migration

Cause

Finding documentation on this specification cannot be found

Resolution

The PME 2024 R3 CM Tool can read from PME systems as far back as PME 7.2. This includes:

Power Monitoring Expert 2024 R1 & R2

Power Monitoring Expert 2023

Power Monitoring Expert 2022

Power Monitoring Expert 2021

Power Monitoring Expert 2020 (9.1)

Power Monitoring Expert 9.0

Power Monitoring Expert 8.X

Power Monitoring Expert 7.2

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: