How can we help you today?

NBRK0250A Rack Access Becomes Inaccessible After Network Cable Removal from Appliance.

Issue:
NBRK0250A Rack Access Becomes Inaccessible After Network Cable Removal from Appliance.

Product Line:
NetBotz 250A

Environment:
Firmware versions v3.2.0.2, v3.3.0.1, v3.4.1.1, v3.4.2.6

Cause: It has been found that leaving the network disconnected from the NBRK0250A causes rack access card swipes to fail after 10 to 15 minutes.

Resolution:
This is being looked at by engineering to be addressed in the future.

Schneider Electric Saudi Arabia