How can we help you today?

Which Contact Block Configurations Can Be Used with 22mm Selector Switches?

Which contact block configurations can be used with 22 mm selector switches?

1. What you need to know

Ø22 mm Harmony selector switches use normally open (NO) and normally closed (NC) contact blocks.

On a 2-position selector switch, a single NO contact is open in one position and closed in the other, while a single NC contact operates inversely, regardless of its mounting position on the fixing collar.

On a 3-position selector, a left NO contact is closed only in the left position, and a right NO contact is closed only in the right position, while center NO is closed in both left and right positions of the selector. A left NC contact is open only in the left position, and a right NC contact is open only in the right position, while center NC is open in both left and right positions of the selector.

2. How contact block position works on Harmony 22 mm selector switches

  • The switching pattern is not an attribute of the contact block itself, but of the combination of contact type (NO or NC) and its position in the fixing collar. The state column reads left to right through the selector positions, with the center position shown only for 3-position devices.
  • The contact block position on the fixing collar is given from the head point of view:Selector switch contact blocks configuration illustration.
  • O = contact open and X = contact closed. For example, O – O – X means the contact is open in the left and center positions and closed in the right.
  • Schneider Electric selector switches comply with IEC 60947-5-1 requirements.

3. Contact block configuration matrix for 22 mm selector switches

Selector typeContact block type and positionContact state according to selector positionWhat you getSample commercial reference
2-position

1 x NO

LEFT or RIGHT

O – XClosed when selector is at the right position.
Example: OFF-ON
Complete unit: XB4BD215
Sub-assemblies: ZB4BD2 head + ZB4BZ101 or ZB4BZ1015 body
2-position

1 x NC

LEFT or RIGHT

X – OOpen when selector is at the right position.
Example: LOCAL-REMOTE
Sub-assemblies: ZB4BD2 head + ZB4BZ102 or ZB4BZ1025 body
2-position

1 x NO + 1 x NC

LEFT and RIGHT

X – XOne contact open for each position.
Example: REVERSE-FORWARD
Complete unit: XB4BD25
Sub-assemblies: ZB4BD2 head + ZB4BZ105 or ZB4BZ1055 body
3-position

1 x NO

LEFT

O – O – XClosed only when selector is at the right position.Sub-assemblies: ZB4BD3 head + ZB4BZ009 fixing collar + ZBE101 or ZBE1015 contact block
3-position

1 x NO

CENTER

O – X – OClosed only when selector is at the center position.Sub-assemblies: ZB4BD3 head + ZB4BZ009 fixing collar + ZBE101 or ZBE1015 contact block
3-position

1 x NO

RIGHT

X – O – OClosed only when selector is at the left position.Sub-assemblies: ZB4BD3 head + ZB4BZ101 or ZB4BZ1015 body
3-position

2 x NO

LEFT and RIGHT

X – O – XOne NO closed when selector is at left or right position.
Example: HAND-OFF-AUTO
Complete unit: XB4BD33
Sub-assemblies: ZB4BD3 head + ZB4BZ103 or ZB4BZ1035 body
3-position

1 x NC

LEFT

X – X – OOpen only when selector is at the right position.Sub-assemblies: ZB4BD3 head + ZB4BZ102 or ZB4BZ1025 body
3-position

1 x NC

CENTER

O – X – OOpen only when selector is at the left and right positions.Sub-assemblies: ZB4BD3 head + ZB4BZ009 fixing collar + ZBE102 or ZBE1025 contact block
3-position

1 x NC

RIGHT

O – X – XOpen only when selector is at the left position.Sub-assemblies: ZB4BD3 head + ZB4BZ009 fixing collar + ZBE102 or ZBE1025 contact block
3-position

2 x NC

LEFT and RIGHT

O – X – OOne NC open when selector is at left or right position.Sub-assemblies: ZB4BD3 head + ZB4BZ104 or ZB4BZ1045 body

Note: NO and NC contact blocks can be combined and stacked in any other way to achieve specific states. The number of stackable elements depends on the contact block reference.

4. Related references

TypeCommercial referenceDescription
Complete unitXB4BD215 Selector switch, metal, black, Ø22, 2 positions, stay put, 1 NO compact push-in terminals
Complete unitXB4BD25Selector switch, metal, black, Ø22, 2 positions, stay put, 1 NO + 1 NC screw clamp terminals
Complete unitXB4BD33Selector switch, metal, black, 22 mm, 3 positions, stay put, 2 NO screw clamp terminals
HeadZB4BD2Black selector switch head, metal, Ø22, 2 positions, stay put
HeadZB4BD3Black selector switch head, metal, Ø22, 3 positions, stay put
BodyZB4BZ101 or 10151 NO contact block with metal fixing collar, screw clamp or compact push-in terminals
BodyZB4BZ102 or 10251 NC contact block with metal fixing collar, screw clamp or compact push-in terminals
BodyZB4BZ103 or 10352 NO contact block with metal fixing collar, screw clamp or compact push-in terminals
BodyZB4BZ104 or 10452 NC contact block with metal fixing collar, screw clamp or compact push-in terminals
BodyZB4BZ105 or 10551 NO + 1 NC contact block with metal fixing collar, screw clamp or compact push-in terminals
Contact blockZBE101 or 1015Single NO contact block, screw clamp or compact push-in terminals
Contact blockZBE102 or 1025Single NC contact block, screw clamp or compact push-in terminals
Fixing collarZB4BZ009Metal fixing collar
  • Note 1: Those products are also available in plastic versions through the XB5 range.
  • Note 2: Selector switch heads and complete units are also available in spring return type, several colors and handle types.

Launch the Product Selector on se.com to configure a Harmony selector switch according to your requirements, or contact Schneider Electric Technical Support to check a configuration against your control scheme.

Schneider Electric Saudi Arabia