How can we help you today?

What should the colours of pushbutton heads typically represent ?

1. What you need to know

According to IEC 60204-1:2021, colors of pushbutton should not be chosen for aesthetic reasons. The purpose is to help operators to easily recognize the function of a pushbutton and act on the machine operation accordingly.
Green is the preferred color for START/ON function ; Red color can be used for STOP/OFF function if not close to an emergency stop device. Blue color can be used for RESET function. Yellow is preferred for ACK/INIT function.

For an emergency stop pushbutton, both IEC 60204-1:2021 and ISO 13850:2015 (Chapter 4.3) specify that the head must be red and the background shall be yellow. This color combination is exclusively reserved for emergency stop pushbuttons

2. Which standards define pushbutton color coding?

  • IEC 60204-1 - Safety of machinery, Electrical equipment of machines. Clause 10.2.1. The primary reference for which color may be used for which actuator function on a machine.
  • ISO 13850 - Emergency stop function. Chapter 4.3 Sets the red actuator on yellow background, the mushroom or palm shape, and the latching principle.
  • NFPA 79 - Electrical Standard for Industrial Machinery applies to the US. NFPA 79 is aligned with IEC 60204-1 for pushbutton colors.

3. Pushbutton color matrix

FunctionPossible colors according to IEC 60204-1Preferred or commonly used colorHarmony XB4 - metal head ⌀22
START/ONWHITE, GREY, BLACK or GREENGREENComplete unit : XB4BA31
STOP/OFFBLACK, GREY, WHITE, or RED if not near to an emergency stop deviceREDComplete unit : XB4BA42
RESETBLUE, WHITE, GREY, or BLACKBLUEComplete unit : XB4BA61
ACKNOWLEDGE or INIT (from abnormal state according to IEC60204-1)YELLOWYELLOWComplete unit : XB4BA51
EMERGENCY STOPRED and YELLOW BACKGROUNDRED and YELLOW BACKGROUNDComplete unit : XB4BS8444
Complete control station with complete unit : XALK178F
OTHER FUNCTIONSWHITE, GREY, or BLACKBLACK or WHITEComplete unit : XB4BA11 (WHITE) or XB4BA21 (BLACK)

4. Schneider Electric references

TypeReferenceProduct description
Complete unit - GREENXB4BA31⌀22 flush Pushbutton, spring return, green, metal, 1NO screw clamp terminals
Complete unit - REDXB4BA42⌀22 flush Pushbutton, spring return, red, metal, 1NC screw clamp terminals
Complete unit - BLUEXB4BA61⌀22 flush Pushbutton, spring return, blue, metal, 1NO screw clamp terminals
Complete unit - YELLOWXB4BA51⌀22 flush Pushbutton, spring return, yellow, metal, 1NO screw clamp terminals
Complete unit - WHITEXB4BA11⌀22 flush Pushbutton, spring return, white, metal, 1NO screw clamp terminals
Complete unit - BLACKXB4BA21⌀22 flush Pushbutton, spring return, black, metal, 1NO screw clamp terminals
Complete unit - EMERGENCY STOPXB4BS8444Emergency stop switching off, metal, red mushroom 40mm, ⌀22,trigger turn to release, 2NC screw clamp terminals
Control station with EMERGENCY STOPXALK178FControl station, plastic, yellow lid, 1 red mushroom push button ⌀40, turn to release, 2NC screw clamp terminals

Note1 : Those products are also available in plastic versions through XB5 range.

Note2 : Pushbuttons exist also in illuminated versions

Launch Product Selector on se.com to configure a Harmony selector switch according to your requirements or contact Schneider Electric Technical Support to check a configuration against your control scheme.

Schneider Electric Saudi Arabia