How can we help you today?

How to program XB4R/XB5R wireless receivers?

1. What you need to know

Programming a Harmony XB5R or XB4R wireless pushbutton has three stages. First set the receiver in pairing mode by pressing the selection button for three seconds. Then select the output on which you want to pair the push button by pressing on the selection button and validate your choice by pressing on the validation button. Then push three times on the pushbutton for teaching it in the receiver; once done the signal LED lights on green steady for two seconds. A ZBRRA receiver holds up to 32 transmitter IDs across its two outputs, the teaching sequence must be completed within 1 minute 30 seconds, and the output becomes active 4 seconds after teaching ends. Full sequences are in instruction sheet S1A57202 and user guide EIO0000000812.

Note : the pairing procedure described in the video is still valid with the current version of receivers.

2. What you are actually configuring

The output function decides what the receiver does when it catches a taught transmitter; it is set per output, not per transmitter. The column that matters most in practice is the third one from the right: some function changes silently erase the IDs already taught to that output, which is the single most common reason a working installation stops responding after a change.

  • The output function is set per output, not per transmitter.
  • Switching an output to or from start/stop erases the IDs already taught to it; monostable ↔ bistable keeps them. This is the most common reason a working installation stops responding after a change.
  • Range is about 100 m in free field, about 25 m with the transmitter in an XALD box and the receiver in a metal enclosure, about 40 m with a ZBRA1 relay antenna.
  • Current approach is a ZBRT1 transmitter with a standard XB4/XB5 head;
  • Documentation: S1A57202 (receiver sequences), EIO0000000812 (full XB5R reference), S1A57198 (transmitter), S1A57194 (relay antenna).

3. Output function comparison

Output functionBehaviourTransmittersEffect of changing to or from itAvailable on
Monostable (default)Momentary - the output follows the press and does not latch1Switching to or from bistable keeps every taught IDZBRRA, ZBRRC
BistableAlternating - one press latches the output on, the next releases it1Switching to or from monostable keeps every taught IDZBRRA
Enable/Disable
(standard)
One transmitter energises the output, a second de-energises it; stop has no priority over start2Switching to or from Enable/Disable clears every ID taught to that outputZBRRA only
Enable/Disable
(advanced)
After stop, start is inhibited until a reset transmitter is pressed2 + resetSwitching to or from Enable/Disable clears every ID taught to that outputZBRRA only

4. Schneider Electric references

FunctionReferenceProduct description
Complete pushbuttonZB5RTA4Red flush wireless and battery less pushbutton, plastic
TransmitterZBRT1Wireless, batteryless transmitter. Current approach: fits under a standard Harmony XB4 or XB5 head.
HeadZB5AA4⌀22 red flush pushbutton head, plastic bezel, spring return. Any standard XB4/XB5 head works.
Fixing collarZB5AZ009Body and fixing collar used to assemble a standard head onto a ZBRT1 (ZB4BZ009 for metal XB4).
Receiver - RelaysZBRRAConfigurable receiver, 2 changeover relay outputs 3 A, 24-240 V AC/DC. Monostable, bistable and enable/disable. Up to 32 transmitter IDs.
Receiver -PNPZBRRCConfigurable receiver, 4 PNP outputs 200 mA, 24 V DC. Monostable only.
AntennaZBRA1Relay antenna with 5 m cable, extends range to about 40 m in metal enclosures (ZBRA3 for passive through-wall).
EnclosureZBRM22Plastic enclosure with 2 cut-outs for mobile or fixed mounting (ZBRM01 for 1 cut-out).

Note : Download the instruction sheet from the product page on se.com, browse the current wireless offer in DigiCat, or contact Schneider Electric technical support to validate a layout before installation.

Explore the Explore Industrial Wireless Remote Control page product range on Schneider Electric's website to select the most suitable solution for your application. If you need assistance verifying compatibility with your control scheme, please contact Schneider Electric Technical Support.