How can we help you today?

Can I choose where exported files are saved in EcoSet Design?

Yes. EcoSet Design allows users to select the destination folder when exporting project files. During the export process, a standard file browser window is displayed, enabling users to specify the desired file name and save location before completing the export.

How It Works

  • Initiate the desired export operation.
  • A file browser dialog opens automatically.
  • Select the destination folder where the exported file will be saved.
  • Enter or modify the file name as required.
  • Complete the export process.

repour

Key Benefits

  • Save exported files directly to a preferred directory.
  • Eliminate the need to search for files in default system locations.
  • Improve document management by organizing exports according to project, customer, or site requirements.
  • Facilitate easier sharing and archiving of project deliverables.
  • Applies to supported export formats such as PDF, DXF, and CSV.

Note: Allowing users to choose the save location provides greater flexibility and helps maintain an organized project documentation structure.