How can we help you today?

How to mount a Harmony 22 mm operator push button?

1. What you need to know

Mounting a Ø22 Harmony operator takes four steps and no tools beyond a screwdriver: insert the head into the Ø22 cut-out from the front of the enclosure, push the mounting collar onto the base of the head from inside with the two arrows aligned until it clicks, tighten the grounding screw, then snap the contact blocks or light module onto the rear of the fixing collar, bottom nub first. The assembly is modular - head, fixing collar and blocks are separate parts - so the fixing collar reference must match the range: ZB4BZ009 for metal XB4, ZB5AZ009 for plastic XB5.

Safety: isolate the panel and confirm no component is energized before starting.

2. Mounting sequence for metal XB4

  1. Insert the operator head from the outside into the Ø22 mm hole, bezel facing the front of the enclosure.
  2. Press the fixing collar firmly onto the base of the head from inside the enclosure, with the arrow on the side of the fixing collar aligned to the arrow on the side of the head. A click confirms that the fork is seated.
  3. Tighten the grounding screw once the operator is in its final position. This step applies to the metal XB4 range only.
  4. Fit the contact blocks or light module: first engage the bottom plastic nub in 1 of the 3 positions of the fixing collar, then push until the metal hooks latch onto the back of the fixing base.

Points that account for most failed assemblies:

  • The arrows are an orientation key, not decoration. If not aligned no possible to install.
  • Complete units (XB4x, XB5x) ship head, fixing collar and block assembled, so only the panel mounting and the grounding screw remain.

3. Mounting sequence for plastic XB5

  1. Insert the operator head from the outside into the Ø22 mm hole, bezel facing the front of the enclosure.
  2. Screw the plastic ring nut, recommended with specific tool (ZB5AZ905),
  3. Place plastic fixing collar on the correct orientation and push till metal clip inside the bezel,
  4. Fit the contact blocks or light module: first engage the bottom plastic nub in 1 of the 3 positions of the fixing collar, then push until the metal hooks latch onto the back of the fixing base.

4. Metal version XB4 vs plastic version XB5

Harmony XB4 / ZB4 - metalHarmony XB5 / ZB5 - plastic
Bezel and collarChromium-plated metalPlastic
Mounting collarZB4BZ009ZB5AZ009
Grounding screwPresent on the fixing collar - tighten once the operator is correctly positionedNot applicable: the plastic body provides double insulation, so there is no earthing step
Panel cut-outØ22 mm, identical for both rangesØ22 mm, identical for both ranges
HeadsZB4Bx heads, metal bezelZB5Ax heads, plastic bezel, plastic ring nut
Contact blocks and light modulesZBE and ZBV - shared across both rangesZBE and ZBV - shared across both ranges
Mounting sequenceSteps 1 to 4 of section 2 aboveStep 1 to 4 of section 3 above

The two ranges share the cut-out, the contact blocks and the light modules. Only the heads and the fixing collar differ - and the grounding step exists on the metal range alone.

5. Example of Schneider Electric references

FunctionReferenceProduct description
Mounting collar - metal (XB4)ZB4BZ009Metal body / fixing collar. Takes up to 3 ZBE contact blocks, or 2 blocks plus 1 light module, and carries the grounding screw.
Mounting collar - plastic (XB5)ZB5AZ009Plastic body/ plastic fixing nut / fixing collar, same function on the XB5 range. No grounding screw.
Head - XB4 metalZB4BA3Ø22 flush head, green, spring return, metal bezel. The last digit sets the color.
Head - XB5 plasticZB5AA3Ø22 flush head, green, spring return, plastic bezel. Fits the same cut-out.
Complete unit - XB4XB4BA31Head, fixing collar and 1 NO contact block supplied assembled - only the panel mounting and the grounding screw remain.
Contact blockZBE1011 NO, screw clamp. Snaps onto the rear of the collar. ZBE102 for 1 NC, ZBE1015 for push-in terminals.
Range - XB4 / ZB4 metalHarmony XB4 / ZB4Modular Ø22 metal push buttons, selector switches and pilot lights.
Range - XB5 / ZB5 plasticHarmony XB5 / ZB5Modular Ø22 plastic push buttons, selector switches and pilot lights.

Instruction sheets are on each product page on se.com; contact Schneider Electric technical support to confirm an assembly before installation.