How can we help you today?

What are the relays state of ZBRRA receiver when powered off?

1. What you need to know

When a Harmony ZBRRA receiver has no supply voltage, both output relays sit in their de-energized position: the NC contacts 11-12 and 21-22 are closed, and the NO contacts outputs 12-14 and 22-24 are open. If the supply is cut off while an output is ON, the contacts outputs return to this same de-energized state. Output states are not retained through a power loss; transmitter pairing and the configured output mode are maintained.

2. Understanding the ZBRRA output behaviour

The ZBRRA is a programmable receiver in the Harmony XB5R (plastic) and XB4R (metal) wireless and battery less pushbutton range. It converts radio frames from ZBRT* wireless batteryless transmitters into dry contact outputs. Its two outputs are electromechanical changeover relays, so their unpowered position is a mechanical rest position, not a saved state.

3. Contact state according to receiver condition

Receiver conditionNC contact
(11-12 / 21-22)
NO contact
(12-14 / 22-24)
Relay state
Not powered (supply off or lost)ClosedOpenDe-energized - default state
Powered, no command receivedClosedOpenDe-energized
Powered, output ON in monostable modeOpenClosedEnergized while the command is active
Powered, output ON in bistable or stop/start modeOpenClosedEnergized until the next command
Supply lost while the output is ONClosedOpenDe-energized - the ON state is not maintained
Supply restoredClosedOpenDe-energized until a new command is received

4. Related references

FunctionReferenceDescription
Programmable receiverZBRRA2 changeover relay outputs 3 A, 24-240 V AC/DC, monostable / bistable / stop-start, 6 indicating LEDs
TransmitterZBRT1Wireless and batteryless transmitter, without head
Transmitter head, plasticZB5RTA2ZB5R plastic pushbutton head, black cap, spring return
Transmitter head, metalZB4RTA2ZB4R metal pushbutton head, black cap, spring return
Visual feedbackZBRV1Visual feedback module for ZBRT transmitters
AntennaZBRA1Relay antenna to extend radio range

Download the instruction sheet from the product page on se.com, browse the current wireless offer in DigiCat, or contact Schneider Electric technical support to validate a layout before installation.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: