How can we help you today?

Do I Need to Purchase Current Transformers (CTs) Separately to Enable SmartAmp™ Load Management?

Product Line
Schneider Charge AC

Environment
Schneider Charge AC with SmartAmp™ Dynamic Load Management

Applicable Products
Schneider Charge with J1772 (Type 1) connector - EVRBA48ANAMJ1772
Schneider Charge with J3400 (NACS/Tesla) connector - EVRBA48ANAMJ3400

Applicable Range
405074973

Answer
No. Current Transformers (CTs) required for SmartAmp™ load management are included with the Schneider Charge charging station. A separate energy monitor is not required for SmartAmp operation.

The included CTs monitor the home's electrical consumption, allowing SmartAmp to dynamically adjust charging current and help prevent exceeding the available electrical service capacity.

CT wiring may be extended when necessary and, where permitted by local electrical codes, can be routed in the same conduit as the AC wiring.

Important: To enable SmartAmp functionality, the charging station must be properly commissioned using the eSetup application.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre