How can we help you today?

Schneider Electric Netmanage Server , Windows Security pop-up asking for Network access permission.

Issue:

Customer installed Machine Expert Basic v1.4 on their Windows 11 PC.

They are getting a prompt about the Schneider Electric Netmanage Server and wanted to know if this can be allowed.

Windows Security prompt

Product Line:

Machine Expert, Machine Expert Basic.

Resolution:

The Windows Security prompt is requesting permission for the Schneider Electric Netmanage Server to communicate through the Windows Firewall.

Windows Network.

If you have to consider Security:

we recommend allowing this application on Private networks only.

Please note that the “Public network” setting does not necessarily mean that the Ethernet connection has Internet access. It is a Windows network profile used for unidentified or untrusted networks. Since the Ethernet connection has no Internet connection and may not be fully identified by Windows, Windows has assigned it the Public network profile by default.

If this Ethernet connection is dedicated to a trusted industrial network, such as a direct connection to a PLC or a controlled machine network, the network profile can be changed as follows:

Windows Settings → Network & Internet → Ethernet → Network profile type → Private

After changing the Ethernet profile to Private, please allow the Schneider Electric Netmanage Server through the firewall for Private networks only and leave Public networks unchecked.

This configuration should allow the required device discovery and Ethernet communication functions while avoiding unnecessary exposure when the PC is connected to an untrusted public network.

If the network profile cannot be changed or automatically returns to Public after restarting the PC, please contact the local IT administrator, as the setting may be controlled by the company’s Windows security policy.

But to ensure maximum compatibility, it is also allowing the application on public networks, provided that the PC is connected to a trusted and controlled network, such as an internal industrial network or a direct connection to a PLC.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre