How can we help you today?

My Smart UPS Modular Ultra UPS runtime did not update immediately when inserting a new Battery Module (BM)

Issue:

Smart UPS Modular Ultra runtime does not update when inserting a new Battery Module (BM) into the system


Product Line:

Smart UPS Modular Ultra


Resolution:

No Action is required.

The battery module will be at a different voltage than the batteries installed in the system (battery bus).  The battery module will not connect (close its discharge FET) to the battery bus if the battery module voltage is higher than the battery bus voltage.  This can happen if the system is on battery or if the system is online recharging previously discharged batteries.  When connected to AC, the system will eventually charge the battery bus to the level of the new battery module.  At that point, the new battery module will connect, and the runtime will update accordingly.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: