How can we help you today?

ION8600 internal modem

Issue

Does the ION8600 internal modem support the V.32 modem standard?

Product

ION8600

Resolution

Yes. The internal analog modem supplied for the ION8600 supports the V.32 modem standard.

The modem was manufactured by Multi-Tech. Refer to pages 30–31 of the attached Multi-Tech technical document for the supported modem standards. See attachment.

Additional Information:

For general information about V.32 and other modem standards, refer to the following Wikipedia article: http://en.wikipedia.org/wiki/List_of_modem_standards

Schneider Electric Saudi Arabia

Attachment(s)
Internal Multitech Modem - AT Commands Rev E.pdf [322.84 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation