How can we help you today?

How to update a Vijeo Designer v4.6 program to version v6.2?

Issue:

Need to update a Vijeo Designer project from version 4.6 to version 6.2.

Product:

Vijeo Designer v4.6, v6.2

Environment:

HMI Configuration Software in Windows

Resolution:

To update a Vijeo Designer v4.6 project to v6.2, the project must first be updated to Vijeo Designer v6.1. Once the project has been successfully updated to v6.1, it can then be updated to Vijeo Designer v6.2.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia