How can we help you today?

CM Tool - not opening with "An error occurred while initializing the system"

Issue

When upgrading or migrating Power Monitoring Expert (PME), the Configuration Manager (CM) Tool doesn't open and shows the following error: "An error occurred while initializing the system. Please see log for more details. The Configuration Manager will now shut down."

CM Tool initialization error

Product Line

StruxureWare Power Monitoring 7.x

Power Monitoring Expert 7.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

CM Tool

Cause

The CM Tool is older than the installed PME version.

Resolution

When upgrading/migrating PME software, always use the CM Tool version matching the target PME version being upgraded/migrated to. Use this same version of the CM Tool on both the old and new application server.

For example, when performing a side-by-side upgrade to PME 2024 R3, use CM Tool 2024 R3 on both the old and new application server.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation