How can we help you today?

SESU v4.0.18.0 does not display available software updates

Question
Why does Schneider Electric Software Update (SESU) v4.0.18.0 not display available software updates?
Answer
This is a known issue in SESU v4.0.18.0. SESU Support is aware of the problem and is working on a fix.
Issue
SESU v4.0.18.0 may fail to retrieve and display available Schneider Electric software updates, although SESU v3.0.12 works correctly in the same environment.
Resolution
As a temporary workaround, uninstall SESU v4.0.18.0 and downgrade to SESU v3.0.12. Use this version until the corrected SESU release is available.

Schneider Electric Saudi Arabia