How can we help you today?

Why is Machine Expert not honoring Forces?

Issue:

Why, if a value was forced to a variable in Machine Expert, this value is not kept by the variable during the execution of the program?

Product Line:

EcoStruxure Machine Expert (all versions).

Resolution:

In the Help documentation of Machine Expert, we have the following information:

Help section about Forcing.

This means that the Force values are only assigned at steps 2 and 4, after reading the inputs and before writing to the outputs.

During step 3, the code is executed and the value of a forced variable can change if a write operation is done to it.

And from the moment that the new value was assigned to the forced variable, this variable will retain this value

and it will be used as is in the rest of the code, until step 4, where the forced value will be reassigned to the variable.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: